AXIS#.PL.AINSCALE

Description

AXIS#.PL.AINSCALE is an analog position scale factor that scales the analog input (AINx.VALUE) for AXIS#.OPMODE = 2 , AXIS#.CMDSOURCE = 3 (analog position mode).

The value entered is the motor position per 1 V of analog input.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Depends on AXIS#.UNIT.PROTARY

Rotary: counts/V,rad/V, deg/V, (Custom Units)/V, 16-bit counts/V

Range

+/- 4,398,046,511,104 counts/V

 

Specific unit ranges are adjusted to account for the above max count range.

Default Value

0 counts/V

Data Type

Float
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
AXIS1.PL.AINSCALE

500ch

07h

Signed32

Position

-

Read/Write

No

AXIS2.PL.AINSCALE

510ch

07h

Signed32

Position

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.PL.AINSCALE

5913

1719

Signed32

Read/Write

Position

AXIS2.PL.AINSCALE

71449

1171

Signed32

Read/Write

Position

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.PL.AINSCALE

5913

Signed32

Read/Write

Position